host端(VCCA)电压为3.3V,SD卡端(VCCB0)电压为1.8V,在SD卡通过CMD信号回复响应的时候,频率提高到3MHz以上的时候3.3V端信号电平无法达到理想电平。在400K的时候没问题。



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
host端(VCCA)电压为3.3V,SD卡端(VCCB0)电压为1.8V,在SD卡通过CMD信号回复响应的时候,频率提高到3MHz以上的时候3.3V端信号电平无法达到理想电平。在400K的时候没问题。



请问这个OD驱动还是推挽驱动,是指SD驱动TXS02612,还是TXS02612设置为推挽输出?
若是TXS02612设置为推挽输出,请问应该如何设置?
CMD线的电容,我不是仅指外接的电容,包括寄生电容等所有电容,如果走线比较长就会形成不可忽略的寄生电容,如果信号速率比较快,电容比较大,那么电容就会在高电平期望充不到期望电平。
表格中的驱动是指外部输入信号驱动TXS02612,也就是是指SD驱动TXS02612的接口类型,TXS02612接口类型不会变,无法设置,如下datasheet截图:

您可以做下交叉验证吗?可以看出TXS02612的Data or Command的转换原理是一样的,你可以将Command信号接在Data 其他管脚看看是什么现象吗