This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: 输出异常

Part Number: TXS0102
Other Parts Discussed in Thread: BQ78350, , BQ76920

您好,

根据图1显示,加入电平转换电路,SMBUS的波形会有问题。摘掉TXS0102DCUR,飞线直接连接,则波形正常。

异常状态如下图2/图3,CPU端发出的波形在低电平时会出现3M的载波,BQ78350端的低电平也显示异常。

 

图2

图3

 

 

  • 您好,

    VCCB电压是2.5V吗?VCCA电压是多少?请确认A 端口的电压在 1.65V 至 3.6V之间,且VCCA ≤ VCCB;

    A 端口和 B 端口上拉电阻接的都是4.7KΩ是吗?如果CPU是发出波形端,那么拆掉 TXS0102后级电路(或者说拆掉BQ78350),用示波器分别看TXS0102输入和输出端波形是否正常?

  • hi TI,

    1,VCCB电压是2.5V,VCCA电压是1.8V。

    2,A 端口和 B 端口上拉电阻接的都是4.7KΩ。与上拉电阻的关系不大,更换过10k和去掉上拉电阻,均没有变化。

    3、拆掉 TXS0102后级电路,TXS0102输入和输出端波形就是正常的。另外,保留BQ78350,摘掉BQ76920( bq76920提供2.5V给BQ78350)是异常的。

    现在看初步的结论就是BQ78350在影响,

    按照BQ78350的SMBUS

    所以BQ78350对应外部CPU(一般外部CPU的接口都是1.8V)的SMBUS接口是否有参考电平转换设计?

    或者不用电平转换,将SMBC SMBD(SMBC and SMBD:“Input/Open-drain output”)与外界1.8V的接口直连,并上拉到1.8V?

  • TXS0102就SMBus 应用的电平转换芯片;

    摘掉BQ76920,您是使用的什么电源给TXS0102 B-port端供电的?

    您可以附上BQ76920+BQ78350+TXS0102 这块的电路吗?我想看下这款的连线情况

  • hi all

    这个问题已经找到原因,是电平转换芯片损伤,

    这个项目是4串联电池,我在测量SMBUS对DIG_GND的电压时发现,当4节电池都放在机器中时,SMBUS对DIG_GND是正常的0V,

    当摘下一节电池,只在电池中放3节电池时,SMBUS对DIG_GND是-5V,这个负压会导致下图中的转换芯片损坏。

  • 很高兴您找到了问题原因,感谢您的反馈。