Other Parts Discussed in Thread: BQ78350, , BQ76920
您好,
根据图1显示,加入电平转换电路,SMBUS的波形会有问题。摘掉TXS0102DCUR,飞线直接连接,则波形正常。
异常状态如下图2/图3,CPU端发出的波形在低电平时会出现3M的载波,BQ78350端的低电平也显示异常。

图2

图3

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi TI,
1,VCCB电压是2.5V,VCCA电压是1.8V。
2,A 端口和 B 端口上拉电阻接的都是4.7KΩ。与上拉电阻的关系不大,更换过10k和去掉上拉电阻,均没有变化。
3、拆掉 TXS0102后级电路,TXS0102输入和输出端波形就是正常的。另外,保留BQ78350,摘掉BQ76920( bq76920提供2.5V给BQ78350)是异常的。
现在看初步的结论就是BQ78350在影响,
按照BQ78350的SMBUS
所以BQ78350对应外部CPU(一般外部CPU的接口都是1.8V)的SMBUS接口是否有参考电平转换设计?
或者不用电平转换,将SMBC SMBD(SMBC and SMBD:“Input/Open-drain output”)与外界1.8V的接口直连,并上拉到1.8V?