74HC245和74LVC245可以互换吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
74HC245和74LVC245功能是一样的,但是它们有多个参数是不一样的,具体是否可以互换,还需确认应用条件;
比如,供电范围不一样:74HC245是2~6V;74LVC245A是1.65 ~ 3.6V;
输入信号范围:74HC245是0 ~ VCC;74LVC245A是 0 ~ 5.5V;
工作温度:74HC245是–40 ~85 °C;74LVC245A是 –40°C TO 125°C;
输出电流:这个与供电电压有关,具体见数据手册,总体来说74LVC245A驱动能力强一些;
74HC245输入端内部集成了钳位二极管,而74LVC245A内部没有等