This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC245A: 74HC245和74LVC245可以互换吗

Part Number: SN74LVC245A


74HC245和74LVC245可以互换吗

  • 您好,

    74HC245和74LVC245功能是一样的,但是它们有多个参数是不一样的,具体是否可以互换,还需确认应用条件;

    比如,供电范围不一样:74HC245是2~6V;74LVC245A是1.65 ~ 3.6V;

    输入信号范围:74HC245是0 ~ VCC;74LVC245A是 0 ~ 5.5V;

    工作温度:74HC245是–40 ~85 °C;74LVC245A是 –40°C TO 125°C;

    输出电流:这个与供电电压有关,具体见数据手册,总体来说74LVC245A驱动能力强一些;

    74HC245输入端内部集成了钳位二极管,而74LVC245A内部没有等