Part Number: SN74ALVC164245
根据手册说明11.1,不用的input需要接VCC或者GND。那output是否也要接VCC或者GND呢?分两种情况:
1. 器件单一方向输出(DIR固定),不用的output是否需要接地?
2. 器件方向可能会切换(DIR根据需要切换),input同时也可能是output,是否都要接地呢?
另外“It is acceptable to float outputs unless the part is a transceiver. If the transceiver has an output enable pin, it will disable the outputs section of the part when asserted. This will not disable the input section of the I/Os so they also cannot float when disabled.” 这句话没有很好的理解,可以解释一下吗?(11.1最后一句)
谢谢