This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: uart信号波形异常

Part Number: LSF0108


Hi,team

我们在调试LSF0108的时候遇到了一个问题。原理图如图所示。

UART1是主板传输过来的串口信号,1.8V电平,位于左边的A端口。希望转换为3.3V后从B端口输出。下图是U10没有上电,在A端口测出的UART1原始波形——

下图是U10上电后,在A端口测出的UART1波形——

可以发现,U10没有上电时,UART原始波形是正常的,但U10上电后,低电平就拉不下来了,按道理低电平应该是0V才对。请问有什么解决手段吗?