Part Number: LSF0108
Hi,team
我们在调试LSF0108的时候遇到了一个问题。原理图如图所示。

UART1是主板传输过来的串口信号,1.8V电平,位于左边的A端口。希望转换为3.3V后从B端口输出。下图是U10没有上电,在A端口测出的UART1原始波形——

下图是U10上电后,在A端口测出的UART1波形——

可以发现,U10没有上电时,UART原始波形是正常的,但U10上电后,低电平就拉不下来了,按道理低电平应该是0V才对。请问有什么解决手段吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不是因为FET上的压降过大造成的,而是A侧驱动端下管导通时(A侧输出低电平)其导通电阻太大的缘故,这样如果B侧上拉电阻较小产生的IB电流就会较大,流过A侧下管导通电阻就会产生较大的压降,使得A侧低电平升高。为了避免这种情况,只能增大B侧上拉电阻以减小IB来减小流过A侧下管产生的压降,如下图示意图,具体分析见视频:https://training.ti.com/translation-lsf-family-0?context=1134826-1139264-1134794