This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD40109B-Q1
3.3V转9V电路怎么设计的?
您好,
真值表如下截图:
电路连接如下:
VCC=3.3V,VCC管脚接供电电源3.3V
VDD=9V,VDD管脚接供电电源9V
输入 A,B,C,D 连接到输入信号
输出E, F, G, H连接到所需的设备/位置
使能管脚 Enable A,B,C,D=VCC连接VCC电压使设备保持使能,或外部控制信号
VSS接地
另外建议在VCC和VDD管脚附件放置0.1 uF滤波电容。