This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD40109B-Q1: 3.3V转9V

Part Number: CD40109B-Q1


3.3V转9V电路怎么设计的?

  • 您好,

    真值表如下截图:

    电路连接如下:

    VCC=3.3V,VCC管脚接供电电源3.3V

    VDD=9V,VDD管脚接供电电源9V

    输入 A,B,C,D 连接到输入信号

    输出E, F, G, H连接到所需的设备/位置

    使能管脚 Enable A,B,C,D=VCC连接VCC电压使设备保持使能,或外部控制信号

    VSS接地

    另外建议在VCC和VDD管脚附件放置0.1 uF滤波电容。