我们将在春节假期期间对网站进行维护,可能暂时无法访问,同时工程师回复将有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: TXB0106 GND脚悬空对信号的影响

Part Number: TXB0106

VCCA为3.3V,VCCB为5V,VCCB与GND脚之间通过一个100nF的电容连接,但GND处于悬空态,未连接到地网络,从测试情况看,5V的方波输入被正确转换为3.3V方波输出,请问长时间来看,GND悬空会有影响吗

  • 您好,

    GND悬空,供电电压和信号没有一个固定的参考点,即使现在能够正常工作,也不能保证以后长期可以正常工作,因为悬空的引脚易受电磁干扰,很容易发生过压】ESD故障。因此不建议让芯片处于这种情况下。