This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: TXB0108B在datasheet中说VCCA<=VCCB,我们单板实测VCCA=3.3V,VCCB=3.1V,不满足要求,想问下有没有对实际使用有什么影响?

Part Number: TXB0108


TXB0108B在datasheet中说VCCA<=VCCB,我们单板实测VCCA=3.3V,VCCB=3.1V,不满足要求,想问下有没有对实际使用有什么影响?

  • 您好,

    要求 VCCA<=VCCB 这是因为当VCCA上的电压超过VCCB上的电压时,内部保护二极管会出现正向偏压,这样会有大量电流流经VCCA并进入二极管,从而增加功耗并可能损坏设备。

    下图是TXB0108 VCCB= 2.5 V, VCCA  从2.5 V 到  3.5 V变化时,流经VCCA的电流,可以看出在在VCCA大于VCCB 0.6V时,VCCA电流随VCCA电压急剧增加。更多详细内容见此文档1.1部分:https://www.ti.com/lit/an/scea060/scea060.pdf

  • 我现在是VCCA=VCCB=3.3V,IO连接的是SPI(四线模式),速率20M,其中CS_N信号在B2端75Kohm上拉,其他信号无上下拉。实际使用总是出现SPI访问FLASH (型号是W25Q512JVFM)失败的情况。试过将SPI直连不经过TXB0108去访问是没问题的,出现访问失败可能有什么原因?

  • 如SPEC 中 8.3.3 Output Load Considerations所描述,TXB0108对输出电容负载有很严格的限制,如果I/O电容负载比较大,输出可能会振荡等异常。TXB0108的I/O走线长吗?是否经过了连接器?走线过长或经过了连接器都会给输出信号线增加容性负载。

    对I/O的驱动也有要求,驱动电流要至少大于±2mA。另外驱动接口是什么类型的?push-pull还是OD/OC?如果是OD/OC驱动接口,TXB系列的转换器不支持,请考虑TXS系列的电平转换。

    您可以附一下TXB0108输入和输出的波形吗?我想看下具体波形是怎样的?