This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
要求 VCCA<=VCCB 这是因为当VCCA上的电压超过VCCB上的电压时,内部保护二极管会出现正向偏压,这样会有大量电流流经VCCA并进入二极管,从而增加功耗并可能损坏设备。
下图是TXB0108 VCCB= 2.5 V, VCCA 从2.5 V 到 3.5 V变化时,流经VCCA的电流,可以看出在在VCCA大于VCCB 0.6V时,VCCA电流随VCCA电压急剧增加。更多详细内容见此文档1.1部分:https://www.ti.com/lit/an/scea060/scea060.pdf
如SPEC 中 8.3.3 Output Load Considerations所描述,TXB0108对输出电容负载有很严格的限制,如果I/O电容负载比较大,输出可能会振荡等异常。TXB0108的I/O走线长吗?是否经过了连接器?走线过长或经过了连接器都会给输出信号线增加容性负载。
对I/O的驱动也有要求,驱动电流要至少大于±2mA。另外驱动接口是什么类型的?push-pull还是OD/OC?如果是OD/OC驱动接口,TXB系列的转换器不支持,请考虑TXS系列的电平转换。
您可以附一下TXB0108输入和输出的波形吗?我想看下具体波形是怎样的?