This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LS273: SN74HCT273N 可以 pin to pin 替换SN74LS273N 么?

Part Number: SN74LS273
Other Parts Discussed in Thread: SN74HCT273

SN74HCT273N 可以 pin to pin 替换SN74LS273N 么?

  • 您好,这两款都是带有清零端的8路D型边沿触发器,功能是一样的,LS指的low-power Schottky Logic。HCT指的是High-speed CMOS  Logic

    电气参数来看,SN 74LS273的工作电压范围4.75V~5.25V。而SN74HCT273的供电电压范围为 4.5 V ~5.5 V。

    另外就是最大时钟频率,传输延迟等这些参数都有差异,具体可对比下二者的数据手册。

    封装来看,SN74HCT273N和SN74LS273N的封装是相同的,引脚排列也是相同的,所以可以替代。 SN74HCT273的数据手册这里打印有误,PIn8和PIn9应该是4Q和4D。打印的是3Q和3D,后续新版的数据手册会更新的。

    综上,二者功能相同,电气参数稍有差异,如果电气参数都满足的话,封装也一样,引脚排列也一样,这二者是可以相互替代的。 并且SN 74LS273这款是非常老的器件了,也建议使用较新的器件来替代。

  • 不客气,那我暂时就先把这个帖子关掉了,后续有其他问题,可以直接跟进或者建个新帖都可以。