Part Number: SN74LS273
Other Parts Discussed in Thread: SN74HCT273
SN74HCT273N 可以 pin to pin 替换SN74LS273N 么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LS273
Other Parts Discussed in Thread: SN74HCT273
SN74HCT273N 可以 pin to pin 替换SN74LS273N 么?
您好,这两款都是带有清零端的8路D型边沿触发器,功能是一样的,LS指的low-power Schottky Logic。HCT指的是High-speed CMOS Logic
电气参数来看,SN 74LS273的工作电压范围4.75V~5.25V。而SN74HCT273的供电电压范围为 4.5 V ~5.5 V。
另外就是最大时钟频率,传输延迟等这些参数都有差异,具体可对比下二者的数据手册。
封装来看,SN74HCT273N和SN74LS273N的封装是相同的,引脚排列也是相同的,所以可以替代。 SN74HCT273的数据手册这里打印有误,PIn8和PIn9应该是4Q和4D。打印的是3Q和3D,后续新版的数据手册会更新的。
综上,二者功能相同,电气参数稍有差异,如果电气参数都满足的话,封装也一样,引脚排列也一样,这二者是可以相互替代的。 并且SN 74LS273这款是非常老的器件了,也建议使用较新的器件来替代。