This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: TXS0108E---------输出波形的电压不满足要求

Part Number: TXS0108E


背景信息:

  1. 我们使用贵司level-shift芯片TXS0108E,目标是把SOC输出的1.8V TDM信号转换为3.3V,(因为AMP TAS6424只支持3.3V逻辑)。
  2. level-shift芯片TXS0108E的后级负载只有AMP TAS6424,且没有下拉电阻。

问题描述:

但是:我们测量发现TXS0108E输出的高电平不是3.3V,最高只有2.5V.

TXS0108E转换芯片有SCKLRCK信号,TXS0108E输出的SCK电平是2.5V(异常),LRCK电平是3.2V(正常)。

 问题分析和结论:

我们debug,把TDM信号的频率由12MHZ降低为1Mhz后(更改SOC输出配置),TXS0108E输出电平由2.5V升高为3V

帮忙支持下,是TXS0108E的驱动能力不足?还是其他原因,导致TXS0108E转换芯片无法支持较高频率?12Mhz频率?

  • 您好,TXS0108E的能支持的信号速率如下:

    TDM信号应该是push pull架构吧?如果是的话,能支持110Mbps。 

    另外,TXS或TXB电平转换的器件确实没有驱动能力,那么针对只能输出2.5V 高电平,想确认下是否有加电阻?或者是否可以断开外围电路,验证下输出是否正常呢?

    这是一篇关于上下拉电阻对TXS或TXB系列器件输出影响的应用手册,可以参考下:

    https://www.ti.com/lit/an/scea054a/scea054a.pdf