This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个是电压转换的电路图,现发现A端口的电压是2.3V,而不是电源电压1.8V。一开始以为是电源芯片5907带载能力不行,查数据手可以输出250mA的电流,排除电源芯片的问题。后来将LSF0204的第1脚即Verv_A脚多线路板上断开,测量A端口电压恢复正常1.8V。用万用表直接测断开的Verv_A脚电压,有2.3V左右的电压,应是输出电压大于5907的输出电压,5907不工作导致。现这种情况不能用,因A口电压大于1.8V。请大家帮我分析下,这样使用对不对,需要做什么调整,谢谢!
您好,
请按照 datasheet 中10.2.1.2.1.1 Pull-Up Resistor Sizing选择上拉电阻值。
在正常工作期间,将有电流从B侧3.3V流入A侧电源1.8V,因此,请确保您的1.8V电源能够吸收这个电流。
下面链接中包含了8个小视频, 讲了LSF系列产品的工作原理,其中第二个视频 Understanding the Bias Circuit for the LSF Family 提到了上述注意事项: