This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVCA164245: SN74AVCA164245

Part Number: SN74AVCA164245


你好,在数据手册中并没有看见这款芯片的外部电路参考设计。请问它的VCCA、VCCB引脚是直接接到对应的VCC值就行吗?不需要额外加个电容滤波?如果需要的话麻烦给一下电容大小。我需要将一个低电平为0V高电平为2.5V的方波(频率为80MHz)进行电平转换,转换成0~1.8V的方波,也即高电平为1.8V低电平为0V的方波(频率为80M)。

下图是数据手册中的测试负载电路。按照我的理解就是芯片的VCCA、B引脚直接接在对应的VCC就行,不需要额外加电容。然后数据输出引脚需要加一个电容CL进行滤波就行