电平芯片从5V转到3.3V脉冲信号,低电平无法拉低到0V左右,最低电平是2V,如图:
输入端5V脉冲,输出端3.3V脉冲
,请问是否遇到过类似问题,如何解决
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
下面链接文档的第2.1部分 Initial Series of TXS Type Devices,讲了 TXS0102的工作原理,如下截图所示:
| A Guide to Voltage Translation With TXS-Type Translators |
看您输入5V波形,低电平是2V,由于输入电压2V小于输出电压3.3V,此时N2 FET是导通的,因此输出也是2V。也就是说输入电压小于期望的输出电压时,输出电压就会跟随输入电压而输出。为了使输出低电平拉低到0V附近,您的输入电压低电平也需要在0V附近。