This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G17-Q1: 脉冲驱动信号下的电流与规格书上定义的有较大出入

Part Number: SN74LVC2G17-Q1
在使用SN74LVC2G17-Q1芯片时遇到以下两个问题想咨询一下:
1、规格书上说对于连续的电流最大是100mA,想问一下对于脉冲宽度30ns,频率为1.1MHz的脉冲信号(VCC=3.3V, VIH=3V, VIL=0V,TA=25°),在使用过程中电流会到163mA大小,想问下在这种条件下器件长时间工作是否有风险;
2、对于脉冲宽度30ns,频率为1.1MHz的脉冲信号(VCC=3.3V, VIH=3V, VIL=0V,TA=25°)。在此条件下测出来VOH=2.459V,但是电流为66.4mA,与下图中给的20mA规格并不相符,想问一下原因是什么?
  • 您好,

    1.是的,有风险。 持续输出电流最大为+-100mA,如果超过这个值,达到163mA的话,将会对器件造成永久性损坏。所以一定要低于这里的最大值。

    2. 您的这两个表格是在数据手册里的吗?我没找到这两个曲线:

    https://www.ti.com.cn/cn/lit/ds/symlink/sn74lvc2g17-q1.pdf

    那么关于Ioh,指的是芯片输出高电平时拉电流的能力,datasheet中给出了它的驱动能力,如下。3.3V供电时, Voh(min)大约在80% Vcc即2.64V左右。 

    您现在测试得到Voh=2.459V, 没有达到输出高电平的最小值,也就是说负载电流过大,直接导致的是它的驱动能力不够。