This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125-Q1: power up issue

Part Number: SN74LVC1G125-Q1

In our design, we have the input of 1P1G125QDCKRQ1 ramping up earlier than it's supply voltage,  will this cause chip damage or abnormal performance?

I also captured oscillating output of this chip while the input kept high, is this phenomena caused by chip damage?

  • 您好,

    In our design, we have the input of 1P1G125QDCKRQ1 ramping up earlier than it's supply voltage,  will this cause chip damage or abnormal performance?

    SN74LVC1G125-Q1支持的推荐输入电压范围到5.5V,因此输入电压大于供电电压是没有问题的。

    I also captured oscillating output of this chip while the input kept high, is this phenomena caused by chip damage?

    SN74LVC1G125-Q1是CMOS输入,如下截图所示CMOS输入结构,当输入沿比较缓慢时,图中的输入端的两个MOSFET有可能会同时导通,这会产生较大的直通电流,若长时间处于这种状态,有可能会烧毁设备。也可能会上下管来回切换导通,这样输出会在低和高状态之间不可控制地振荡。因此,对于这种CMOS器件,数据表定义了防止发生这种情况的最小输入变化速率Δt/Δv ,SN74LVC1G125-Q1的如下截图所示。

    您所附输出波形振荡很可能是由于输入信号沿太缓慢造成的,因此建议您检查输入信号的斜率是否满足datasheet 要求。

    更多相关信息见应用手册: