This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: 电压电平转换器TXS0108E的VCCA与通道A之间的阻抗是46KΩ还是4.6kΩ?

Part Number: TXS0108E

三个一模一样的TXS0108E芯片,不上电时测试VCCA与A通道之间的阻抗(芯片1和2脚),有两只显示46KΩ,最后一只约4.6KΩ。 VCCA是1V8供电的,我们1V8的阻抗出现了异常(降低),是不是4.6KΩ这个芯片损坏了?

  • 您好,

    看下面文档我截图处所描述的工作原理,TXS0108E是smart 上拉电阻,它会动态改变上拉电阻值,当VCCA or VCCB 是 0 V时,I/O是高阻态。我不清楚您具体是怎样测量的?我理解此时用万用表测量阻抗的话应该是无穷大。

    VCCA是1V8供电的,我们1V8的阻抗出现了异常(降低),是不是4.6KΩ这个芯片损坏了?

    “ 1V8的阻抗出现了异常(降低)” 这里具体是什么意思?

    4.6KΩ这个芯片还有哪些异常现象?

x 出现错误。请重试或与管理员联系。