Part Number: TXS0108E
三个一模一样的TXS0108E芯片,不上电时测试VCCA与A通道之间的阻抗(芯片1和2脚),有两只显示46KΩ,最后一只约4.6KΩ。 VCCA是1V8供电的,我们1V8的阻抗出现了异常(降低),是不是4.6KΩ这个芯片损坏了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
看下面文档我截图处所描述的工作原理,TXS0108E是smart 上拉电阻,它会动态改变上拉电阻值,当VCCA or VCCB 是 0 V时,I/O是高阻态。我不清楚您具体是怎样测量的?我理解此时用万用表测量阻抗的话应该是无穷大。
| A Guide to Voltage Translation With TXS-Type Translators |

VCCA是1V8供电的,我们1V8的阻抗出现了异常(降低),是不是4.6KΩ这个芯片损坏了?
“ 1V8的阻抗出现了异常(降低)” 这里具体是什么意思?
4.6KΩ这个芯片还有哪些异常现象?