Other Parts Discussed in Thread: HD3SS3411, HD3SS3412
Dear Supporters,
Need to find a High speed differential 1:2 switch IC solution for IVI application.
The requirements are as follows: block diagram.

Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello please refer to HD3SS3411 which has a bandwidth of 7.5 GHz, and it is used for FPD Link, LVDS, PCIE Gen II, III, XAUI and USB3.1.
Please check the IO voltage if it meets your requirement , the bandwidth should be enough for your application.
https://www.ti.com/product/HD3SS3411

you mean 4PDT which indicates 4 channel with SPDT differential high speed switch?
If yes, please refer to HD3SS3412:
https://www.ti.com/lit/ds/symlink/hd3ss3412.pdf
Please refer to its function diagram if it meets your requirement:

Differential switch could be used for switch differential signal, it also belongs to analog switch.
In addition, analog switch could be also used to switch digital signal, "Analog" just means that all voltages between GND and VCC can be switched. Analog switch is also fine for digital signals.