This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: SPI使用电平转换异常

Part Number: LSF0204
Other Parts Discussed in Thread: TXU0304, TXB0104

你好!
用LSF0204芯片来转换SPI信号,现在B端电压无法到3.3V和A端1.8V电平一样?原理图如下,疑问如下:
1、此芯片是否可以用来转换SPI信号?手册中写的是SPI.MDIO,此处是打印错误吗,这是什么接口信号呢?应该是SPI和MDIO?
2、此芯片A和B端都需要加上拉电阻吗?只从A端调CPU上GPIO驱动能力是否可以?
3、为什么从CPU端调大GPIO驱动能力到10mA,B端输出电压还是1.8V?