This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LXC8T245: 上电过程中IO输出存在高电平。

Part Number: SN74LXC8T245


使用SN74LXC8T245PWR逻辑芯片在上电过程中存在20US的高电平。

1、供电情况:VCCA(+3.3V)由VCCB(+5Vdc)通过LM26420XMH芯片产生;

2、数据方向:Data-A到Data-B;

3、Data-A采用10K电阻下拉;

以下是上电过程中VCCA/VCCB/A8/B8同步的波形:

这个上电中的脉冲高电平是怎么产生的?是哪地方设计不合理吗?

谢谢。