Part Number: SN74HCT574
Customer test NXP's 74HCT574PW, 118 and TI's SN74HCT574PW and found that the initial output level of power-on is not the same as that of power-on, everything is normal

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HCT574
Customer test NXP's 74HCT574PW, 118 and TI's SN74HCT574PW and found that the initial output level of power-on is not the same as that of power-on, everything is normal

Hello ,
We do not familiar with NXP chip, please describe your issue about SN74HCT574 data sheet, product information and support | TI.com.
The customer connects the OE pin to ground, the output Q level is high at the initial moment of power-up, and the output level becomes low after the program is initialized, how can the output be guaranteed to be low at the initial moment?
Hello,
Regarding “Table 6-1. Function Table”, it is hard to guarantee if OE is enabled all the time.
Or you may try to connect a pull down resistor in output pin .

What is different between OUTPUT Q0 & Z? The customer connects the OE pin to ground, the output Q level is high at the initial moment of power-up, and the output level becomes low after the program is initialized, how can the output be guaranteed to be low at the initial moment? (can't add pull-down resistor)
Hello ,
Z means HI-Z, Q0 means previous output.
We suggest you use pull-down resistor to guarantee initial low if OE is enabled when power up.