This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC4060: The period of DQ signal is not 16 times that of the CLKO .

Part Number: SN74HC4060

The period of the waveform output at the DQ signal terminal is not 16 times that of the CLKO terminal.The RC parameters are as follows:R1=56KΩ,R2=240KΩ,C=3400pF.The  supply voltage is 5.3V.