• LSF0108: 双向通信,速率提高到50MHz时出现写入数据和读取数据不一致的问题

    Part Number: LSF0108
    Other Parts Discussed in Thread: TXB0304

           hi 你好,使用LSF0108进行1.2V和3.3V电平信号转换,用于QSPI信号双向通信,目标速率是50MHz,但当速率提高到50MHz会出现写入数据和读取数据不一致的问题,目前实测最大速率只能支持到33.33MHz时数据和读取数据是一致的,参考电路图如下,实测时A侧的上拉是去掉的,为了增大驱动能力B侧的上拉换成了330Ω,还请看下什么原因导致的速率提高到50MHz时出现写入数据和读取数据不一致…

  • TXS0108E: TXS0108的VCCA端口输出电压是否支持1.2V。

    Part Number: TXS0108E
    Other Parts Discussed in Thread: TXB0108, LSF0108, TXB0304, TXB0302

    TXS0108在Datasheet中描述VCCA的Input Power最小为1.4V,在TXS0108的ibis模型中有VCCA为1.2V的模型,请问VCCA是否支持1.2V?

  • TXB0304EVM: TXB0304 EVM 测试,输出波形振铃和跌落电压较大。

    Part Number: TXB0304EVM
    Other Parts Discussed in Thread: TXB0304

    测试环境说明如下:

    1、输入通道CH B、输入信号频率500kHz、电压1.2V,输出通道CH A、电压1.8V;

    2、OE跟VCCA接到一起,然后接到1.8V电源上;

    3、1.2V、1.8V电源接到外部程控电源上;

    4、测试波形如下:

  • TXB0304: TXB0304的输入输出问题

    Part Number: TXB0304

    请问各位大佬们,对于TXB0304,我在datasheet中看到A1和B4均位input/output1,那是不是表示当A1为input1时,对应的output为B4,是我理解有问题吗?请各位解惑。按照常理来说,A1为input,对应的同一侧的同一处引脚为output。

  • TXB0304: TXB0304

    Part Number: TXB0304

    组网环境:OE=H(使能)、VCCA=1.2V、VCCB=1.2V、输入端口A1pin的电平从2V到3.6V变化,观察VCCA pin以及 A1 pin流过的电流

    结果:(Ipad为A1 pin的电流) 随着输入pin电压的变化,VCCA以及输入pin上的电流不变。

    VCCA VPAD IVCCA(mA) IPAD(mA)
    1.2 2 23.44 23.98
    2.1 37.43 38.57
    2.2 37.45 38.78
    2.3 37…
  • TXB0104: 最高速率负载电容条件咨询

    Part Number: TXB0104
    Other Parts Discussed in Thread: LSF0204, TXB0304,

    Hi all,

    我是一名硬件工程师,目前在考虑使用该款双向电平转换芯片作为1.8V to 3.3V QSPI的双向电平转换,最高速率需要达到50MHz,需要启到隔离的效果,所以关于该器件我有几个问题想要咨询:

    1. 请问能否提供最大速率下对于电容的要求,我看到该器件建议最大负载电容不能超过70pF,请问这是什么速率下的电容?我还看到最高速率时的测试条件为15pF电容…

  • LSF0204: 上拉电阻选择以及是否可以用于推挽的双向数据传输

    Part Number: LSF0204
    Other Parts Discussed in Thread: SN74AVC8T245, TXB0304

    我们有一个8bit 的60Mhz的信号(双向传输,两边的输入输出都是push-pull mode),需要在3V3和1V8之间转换,目前看到只有LSF系列可以满足;但是看到手册里一段话感到有些疑惑,LSF是对于push-pull的器件只能用于单一方向的传输吗?

    另外,对于推挽的双向传输,是不是只需要在B port增加pullup(200ohm)即可…

  • TXB0304: Output abnormal when TXB0304 output to MUX IC TS3A27518E

    Part Number: TXB0304
    Other Parts Discussed in Thread: TS3A27518E, SN74AXC4T774, SN74AXC8T245

    Hi Sir,

    Please ref attach pic.

    In our SPI topology CPU(1.8V) <=> TXB0304 <=> TS3A27518E(3.3V), SPI CLK is abnormal at TXB0304 output.

    If we cut off…