This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] XTR116:无法在 XTR116 的输出负载处测量电压。

Guru**** 2815985 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1587200/xtr116-voltage-could-not-be-measured-at-the-output-load-of-the-xtr116

器件型号: XTR116

电压应该为 2.5V、但我测得的值仅为 160mV、并且它不会随输入电压的变化而变化。

我检查了 VREG = 5V、VREF = 4.11。

这几乎和典型应用一样,我是否有误解?

 

image.png