Other Parts Discussed in Thread: LMH6521, ADC34J45, LMH6522, ADS41B49, TINA-TI
主题中讨论的其他部件:ADC34J45,LMH6521 , TIDA-0.0073万, ADS41B49, TINA-TI
您好,
我的设计将包括ADC34J45,它将具有与Altera Arria 10 FPGA的JESD204B接口。
四个模拟输入将由LMH6522放大器放大。
模拟信号输入的频率有2种,分别为189MHz或236MHz。
模拟输入参数包括:
- 单端
- 频率:189MHz或236MHz。
- 带宽:30MHz
- 50欧姆。
采样率与输入频率分别为108MHz或135MHz (Nyquist4)。
请告知LMH6522和ADC34J45之间的建议阻抗匹配是什么,以及之间的建议阻抗匹配是什么
单端输入信号(50欧姆)和LMH6522?
谢谢!
David Siksik