主题中讨论的其他部件: TRF37C73
大家好,
我正在考虑使用TRF37C75 替换1.3GHz无线电PA。 TRF37C75的性能令人印象深刻。 但是,这需要一点力量。
是否可以降低主动偏置电源(针脚1)上的电压以降低电源电流? 我会将典型 的Vcc (4-5V)保留在RFout引脚上。
谢谢!
海登
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hayden,
此时,我认为如果设备在3.5V直流偏压下运行,则没有已知异常或行为。 我不建议低于3V,正如您在测量中所指出的那样,射频输出功率会大大低于3V。 但是,我想重申的是,这些部件未在建议的4.5V工作电压下进行测试,任何不符合预期的行为都是您在建议的工作范围之外操作设备时必须小心的。
您是否看过适用于您的应用的TRF37C73? 我认为这款设备非常适合您使用3.3V电源和16.5dBm射频输出功率来实现的目标。