主题中讨论的其他部件: TINA-TI
参考附加的模拟,我使用的是ADA4841的输出后的OPA1632。 ADA4841的输出具有2.2Vpp的输出和1.78V的偏移,我正在将输出连接到OPA1632,该OPA1632具有Unity增益,仅用于从单端输出到差动输出。 我已经给了2.2 Vpp,并且每侧都得到1 V电压,所以这很好,但是我要求两个输出上的最大峰值不应超过2.8V,但是R9的输出已达到3.79 ,如simution中所示。 请建议如何将我的输出调整到2.8V峰值范围内。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考附加的模拟,我使用的是ADA4841的输出后的OPA1632。 ADA4841的输出具有2.2Vpp的输出和1.78V的偏移,我正在将输出连接到OPA1632,该OPA1632具有Unity增益,仅用于从单端输出到差动输出。 我已经给了2.2 Vpp,并且每侧都得到1 V电压,所以这很好,但是我要求两个输出上的最大峰值不应超过2.8V,但是R9的输出已达到3.79 ,如simution中所示。 请建议如何将我的输出调整到2.8V峰值范围内。
您好Kiran,
您看到R9的OPA1632输出达到3.79V峰值的主要原因是R7 (1.78V)和 R5 (GND)的OPA1632输入之间的DC偏移。 这可以通过在两个输入端应用类似的DC电平或使R5端的DC电平 与R7 (或1.78V)相同来纠正。 这样,就没有输入直流偏移, 而OPA1632输出都 围绕 默认输出共模电压(或原理图中的2.5V)进行居中。
由于您提到最大输出峰值限制为2.8V,因此需要将输出共模直流电压降低至2.2V。 这可以通过将OPA1632 Vocm引脚绑定到2.2V来实现,这将导致 在2.2V周围出现0.5V峰值的最大摆幅 ,或将2.7V作为最大峰值电压。
我附上了TINA-TI示意图,如果您想查看它的话,请附上更正内容。
此致,
Rohit