Other Parts Discussed in Thread: TLV272, LM358
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMV358 主题中讨论的其他部件:TLV272, LM358
正在寻找与 LMV358IDGKR类似的替换产品(相同的引脚),但对于Vcc=10V或更高版本,低成本操作系统约为0.1美元
找到 TLV272,但价格太高
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好Eli:
以下是一个常见问题帖子,可能也会有所帮助: