请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TL074 由于客户错误,TL074的反馈电阻器未连接(打开)。
这种情况是否可能导致TL074损坏?
【背景】
・电路连接在上方。(Vcc为±15V)
・第二次,反馈电阻器正确连接10kΩ Ω,但输出异常。
・我想知道TL074损坏的可能性,因为应该判断TL074故障或异常输出的外部原因。
此致,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.