Other Parts Discussed in Thread: OPA227, OPA192
大家好,
我想找到一个运算放大器来取代ST TSX711A,但使用更宽的电源电压范围。 我只是在网站上找到了OPA189DBV。但是,它只是预览。
您是否可以建议更换一个?
谢谢!
钟
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Bell:
根据您可能最感兴趣的设备规格,我为您提供了几种不同的建议。
OPA192 - 36V电源, 更宽的10MHz带宽,低输入偏移电压(最大25 µV)和漂移(0.15 µV /°C),1 mA静态电流消耗
OPA227 - 36V电源,更宽的8 MHz带宽, 低输入偏移电压(最大75 µV)和漂移(0.1 µV /°C),低3 NV/√Hz宽带电压噪声
OPA192是两者中功耗较低的替代产品,OPA227提供了更好的噪声性能-与具有更宽36V电源额定值的TSX711相比,两者都显著提高了直流和交流性能。
如果您对上述设备有任何疑问,或者有任何其他设计限制,请告诉我,我们应该考虑这些限制。
---
Christopher Stemple
产品营销-精密放大器