请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:XTR111 你好。
我想将XTR111用于一个安全关键型铁路应用。
我们通过在输出20/5mA (频率为25 Hz)上的曲率对信号进行编码。
我们有一个非常重要的问题,即XTR111是否可以在不影响输入的情况下生成输出信号。
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.