您好,
我们正在使用OPA551 (SO-8封装)来生成+/- 24V的波形(通过DAC控制)。 但是,当我们将电源的+24V连接到V+(引脚7),将-24V连接到V-(引脚1,4和5)时,如果有或没有任何类型的输入,功耗约为140mA。 我们的输出电流仅限于2mA。 IC与100nF和10nF电容器分离。
最终,OPA551工作完美,但唯一的问题是,说实话,功耗极高。 是否有解决此问题的简单方法? 我已经试过几次芯片,但结果都是一样的。
谢谢!
- Raoul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我们正在使用OPA551 (SO-8封装)来生成+/- 24V的波形(通过DAC控制)。 但是,当我们将电源的+24V连接到V+(引脚7),将-24V连接到V-(引脚1,4和5)时,如果有或没有任何类型的输入,功耗约为140mA。 我们的输出电流仅限于2mA。 IC与100nF和10nF电容器分离。
最终,OPA551工作完美,但唯一的问题是,说实话,功耗极高。 是否有解决此问题的简单方法? 我已经试过几次芯片,但结果都是一样的。
谢谢!
- Raoul