Other Parts Discussed in Thread: THS7376
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:THS7376 大家好,
客户希望将THS7376用于VGA 1-2缓冲区应用。
能否请您提供您对该原理图的意见?
巴西,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我确认此结构图。
1.是的
2.这取决于Pi衰减器。 在BMC (BNC?)上 输入时,您必须将75欧姆电阻接地。 如果Pi衰减器的输入为75欧姆,则不需要此电阻器。
3.如果布局紧凑,则不必担心进行迹线75Ω。以下是一些指南。
此致,
Sean