Other Parts Discussed in Thread: OPA2197, LM2903
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:OPA2197, LM2903
我想计算IC703 (OPA2197)的VOL。 运算放大器的容积取决于负载。 那么,上面显示的比较器电路的Rin是什么? R737电阻为2.49千欧。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好Yee,
请看一下此模拟:
你可以看到,100k电阻器上没有相关的压降。 因此,LM2903的输入是非常高的电阻。
比较器的Rin以C728为主。 但1nF电容的阻抗仅在极高频率下相关。 1kHz时1nF电容的阻抗为160kOhm,10kHz时为16kOhm。
Kai