请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LM2904 大家好,
VCC的绝对最大额定电压在数据表中声明为±13或26 V。
我的客户想要使用Vcc=3.3V,GND=-15V。
如果有问题,请告诉我问题的原因。
VCC-GND=VCC-(-15)=18 3.3 < 26。
此致
Koji Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.