This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AMC1311:不同的VCC

Guru**** 2834805 points

Other Parts Discussed in Thread: AMC1311, ISO7763

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1096426/amc1311-different-vcc

部件号:AMC1311
主题中讨论的其他部件: ISO7763

大家好,

AMC1311和ISO7763这些隔离设备是否使用不同的VCC?  

例如 VCC1=3.3V,VCC2=5V