Other Parts Discussed in Thread: INA226
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:INA226 分流电阻器之间的电压是否限制在82mV 左右、如下所示?
是否可以将其用于分流电阻的配置:1Ω Ω、电流:最大0.7A、如下所示?
此外、在上述条件下、它是否会影响电流监控器的功能和精度?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.