This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA455:OPA455 -是否可以在负轨上使用-150V 电源?

Guru**** 2788735 points

Other Parts Discussed in Thread: OPA455, OPA462

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1054214/opa455-opa455---can-power-w--150v-on-neg-rail

器件型号:OPA455
主题中讨论的其他器件: OPA462

您好!

对于 OPA455 -在正电源轨上为0V (GND)和负电源轨上为-150V 的器件供电是否电气正常?

我有一个应用、在该应用中使用两个 OPA455将是有益的-一个驱动信号的正极部分、另一个驱动负极-我需要驱动的信号
需要~+100V 和~-100V。

在这些条件下、该器件是否能够向2K 欧姆的负载提供~45mA 的电流?

谢谢!
约翰·W