Other Parts Discussed in Thread: OPA858
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:OPA858 您好、专家、
我的客户使用 OPA858设计了一个 TIA 应用、直流增益为30K、交流增益为100K、当 PD 收到光时、输出中没有交流信号。 您能提供一些建议吗?

BR
CHI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.