Other Parts Discussed in Thread: LM339, OPA350
主题中讨论的其他器件:LM339、
大家好、团队、
我的客户遵循两种配置。
在这两种情况下、10A 直流电流通过感应电阻器。
但上图的输出高达4V、下图为2.59V。
在我的上图计算中、电压应为5V (最高 Vcc)、低于2.75V。
您能否估计输出为何不遵循我的计算?
两个负载均为 LM339 (比较器)的7引脚(1IN+)。
此致、
Koyo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.