主题中讨论的其他器件: OPA659
您好!
如何使用 OPA836实现缓冲器?
我附加了我的仿真、请看一下。
运算放大器在5V 单电源下运行。
输入信号为直流到60MHz、振幅为1V。
R1和 R3用作衰减器、输入阻抗必须为1M 欧姆。
我遵循了 OPA836数据表中图60的原理图。 我的仿真是基准电压为1V 的同相单电源。
但输出信号似乎是错误的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.