请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:INA126 主题中讨论的其他器件: OP27
您好!
我使用增益为368 (RG = 220欧姆)的 INA126。 基准引脚的输入约为6.5VDC。 我的输出摆动6 mv! 但是、当我将 RG 更改为500欧姆(增益较小)时、输出就像摇滚一样稳定。 有什么想法,原因是什么? 谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.