Other Parts Discussed in Thread: TL082
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TL082 您好!
客户使用 TL082进行电流检测。
它们将为 TL082提供5V 和-5V、但-5V 将延迟100ms。
持续时间为100ms、无信号输入、但输出将为5V、可能的原因是什么?
谢谢!
陈义山
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.