This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSPM0C1104:是否有办法取消对此芯片的砖化?

Guru**** 2952510 points

Other Parts Discussed in Thread: MSPM0C1104, MSP-FET

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1503525/mspm0c1104-is-there-a-way-to-unbrick-this-chip

器件型号:MSPM0C1104
主题中讨论的其他器件: MSP-FET

工具/软件:

MSPM0C1104芯片。 特别是8引脚型号、目的是使用 BGA 版本。  

我正在使用 LaunchPad 开发套件进行开发、并已开始针对采用 SOT 封装的8引脚版本推出产品。  但是、我遇到了编程问题、似乎我已经试过两个芯片。

我得到的调试器输出为:

Error connecting to the target:  Connection to MSPM0 core failed.  Possible root causes: 1) Debug access within NONMAIN was disabled or enabled with password. 2) Peripheral mis-configuration (e.g improper watchdog or clock).  To see a more detailed diagnostic of the issue, please press the 'Read boot diagnostic' button.

和  

CS_DAP_0: Device diagnostic read = 0x00000007 
CS_DAP_0: 
Possible root causes from diagnostic reading:
1) Nested exception (e.g double hard fault or NMI) can be caused by illegal CPU activity such as invalid address modification
2) Debug access has been disabled

Possible recovery method:
1) Perform a DSSM factory reset with or without password
2) Power cycle or reset the device

我已经尝试了下电上电、对 LaunchPad/XDS110下电上电、对两者下电上电、仔细检查连接、减小 TCLK 等

是否有办法保证设备恢复?   

我已经验证使用新芯片时连接是否正常、但我无法承受在进入产品时深度拆焊和重新焊接芯片、尤其是如果我要使用 BGA 封装。   

我也确实做到了 不会 重新使用 NRST、SWDIO 和 SWDCLK 线、确保不会与编程引脚发生任何冲突。  

我还将尝试使用一个 JLink Plus 和一个 MSP-FET、看看它们是否能提供帮助。